Ruckus为TestBird创新手游自动化测试提供技术保障

高容量、高密度并发接入及抗同频干扰能力 令Ruckus成为TestBird无线网络设备供应商
2014年7月28日 America/Los_Angeles

北京,7月28日 - 智能无线网络公司优科无线(Ruckus Wireless,Inc. 纽交所代码:RKUS)日前宣布,领先的手游自动化云测平台TestBird采用了Ruckus 无线网络设备,助力其手游自动化云测平台成功运营。TestBird使用了Ruckus ZoneFlex 7982接入点,通过单一接入点为其测试环境中200余个各类型手机终端提供稳定可靠的无线网络接入,为TestBird手游自动化云测平台的商用运营提供了坚实保障。

TestBird隶属成都中云天下科技有限公司,专为手游开发商和渠道提供技术支撑服务。当前,手游产业面临井喷式增长,根据第三方机构艾媒咨询发布的手游市场报告显示,2013年中国手游市场规模达到122.5亿元,同比增长108.7%,中国手游用户规模达到3.85亿,同比增长34.6%,预计2014年手游市场规模将超过190亿元,用户规模将超过4.5亿。中国手游市场发展如此迅猛,而开发商则遭遇游戏品质提升的挑战,包括手机终端兼容性、屏幕适配、动态画面处理等。由于开发商的测试能力有限,往往无法发现游戏和各种终端的兼容性和性能问题,从而导致用户流失。TestBird依托超过200款各种型号智能手机终端的真机测试环境,提供100%基于Web的SaaS云服务,将手游的质量提升一个台阶,有利于手游厂商在竞争中胜出。但由于Wi-Fi工作在免授权频段,不同设备使用同一信道或是同一无线频段发射与接收Wi-Fi信号时的设备之间存在相互干扰现象,即所谓的Wi-Fi的同频干扰问题。因此,为了搭建TestBird手游自动化云测平台的真机测试环境,中云天下需要稳定、可靠、能支持高并发连接的无线网络接入点,为真机测试环境中的200余台各类型智能手机终端提供无线网络连接。

成都中云天下科技有限公司技术总监邓飞表示:“搭建真机测试环境的最大挑战,在于不同手机设备之间的同频干扰,以及同时有数百部不同型号手机设备对高密度稳定接入的要求。TestBird真机测试环境要求同时接入200余个不同型号的智能手机,并通过Wi-Fi无线网络与服务器端连接并进行实时的数据互动。使用传统Wi-Fi接入点时,单个AP的并发接入数较少,因此往往需要5-6台AP才能满足接入要求,但随之而来的相邻AP之间的同频干扰就十分严重,而采用了Ruckus智能无线Wi-Fi接入点后,解决了高密度Wi-Fi手机设备连网的问题,为TestBird商用运营提供了稳定、可靠的基础。”

Wi-Fi同频干扰问题之所以会出现,那是因为在中国2.4G频段下总共有13个可用信道,但仅有1、6、11三个信道没有重叠的频段,因此通常认为在2.4G频段下相互不干扰的信道为1、6、11。如果在同一空间中同时有4台AP工作,那么至少有两台AP的信道会出现重叠,即多个设备可能会在同一频段下工作,不同AP间传输的不同数据会在相同的频段内相互冲突、干扰,造成无线网络接入困难、带宽下降等问题,同一频段下同时工作的AP越多,同频干扰问题也就越严重。举个生活中的例子,假如用户在开车时收听北京交通广播FM103.9,而其旁边的车载MP3也采用103.9频段,那么用户同时会听到广播和MP3的声音。因此,对于TestBird来说,单个AP的并发接入数对于信号的稳定显得尤为重要,其部署的AP能实现的接入数越多,那么Wi-Fi环境则更加平稳,干扰问题不复存在。

TestBird所采用的Ruckus ZoneFlex 7982 是专为高密度并发、高性能和干扰严重的环境而设计,集成的Ruckus 专利 BeamFlex™自适应天线阵列技术和ChannelFly™信道选择技术,能有效减少同频干扰,每个接入点最多可支持500个并发Wi-Fi 客户端。Ruckus专利的自适应天线阵列BeamFlex™将有限的发射功率聚成束状,可以跟踪终端设备的方位,既可以实时降低其它Wi-Fi网络干扰,也可以避免无线信号无目的发射造成的干扰。同时Ruckus的ChannelFly™功能可以实时动态监测干扰,并充分利用全部可用的频谱资源,为终端设备提供稳定可靠的接入,有效降低了干扰。

此外,ZoneFlex 7982可支持画质最好的高清视频,同时支持对服务质量要求苛刻的语音和数据应用,是数据量高的流媒体应用的最佳选择,能充分满足高密度手游真机测试中涉及到的视频、声音、图像等数据传输需求。这正是Ruckus此次被TestBird选为供应商的重要原因。

Ruckus拥有丰富的为企业客户部署高密度Wi-Fi无线网络连接的经验。在此之前,Ruckus还曾帮助北京首都机场和广州白云机场部署智能Wi-Fi无线网络。首都机场旅客年吞吐量超过8369万人次,白云机场年吞吐量超过5265万人次,旅客规模庞大。Ruckus的智能Wi-Fi网络成功给予首都机场T3航站楼和白云机场的所有旅客以及机场的数字标牌等应用提供了全方位支持,实现了Wi-Fi信号的广泛覆盖并避免了信号的干扰。

ABOUT RUCKUS WIRELESS

Headquartered in Sunnyvale, CA, Ruckus Wireless, Inc. (NYSE: RKUS) is a global supplier of advanced wireless systems for the rapidly expanding mobile Internet infrastructure market. The company offers a wide range of indoor and outdoor “Smart Wi-Fi” products to mobile carriers, broadband service providers, and corporate enterprises, and has over 36,000 end-customers worldwide. Ruckus technology addresses Wi-Fi capacity and coverage challenges caused by the ever-increasing amount of traffic on wireless networks due to accelerated adoption of mobile devices such as smartphones and tablets. Ruckus invented and has patented state-of-the-art wireless voice, video, and data technology innovations, such as adaptive antenna arrays that extend signal range, increase client data rates, and avoid interference, providing consistent and reliable distribution of delay-sensitive multimedia content and services over standard 802.11 Wi-Fi. For more information, visit https://www.ruckuswireless.com.

News Media Contact

カテゴリ

Ruckus