CommScope Introduces New ConQuest® Conduit Design for Multiple Cable Installations

Capable of Providing Additional Pathways for Future Use
March 30, 2011 HICKORY, N.C.

CommScope, Inc., a global leader in infrastructure solutions for communications networks, has introduced a new ConQuest® conduit design capable of simplifying installation and management of multiple cables in a single duct.

The new ConQuest® Detectable SubDuct conduit, with its innovative design, targets underground cable networks having current and future cable capacity requirements. As a simple and cost-effective solution, it allows end-users to install a single-duct solution today that provides additional capacity for future cable installations. This forward planning eliminates the need to place additional dedicated conduit later as the network expands. Each separate pathway is capable of carrying individual cables while protecting against natural or construction-related damage.

“CommScope’s SubDuct conduit establishes a throughway for end-users to place multiple cables independently during a single installation,” said Douglas Wells, director, Broadband, Hybrid Fiber Coax, CommScope. “With the company’s proven track record for designing award-winning conduit solutions for our customers, we believe this design provides them additional options when installing today’s rapidly changing and expanding networks.”

ConQuest® Detectable SubDuct’s unique design allows it to be customized with various amounts of three-quarter inch chambers within a single jacket, providing easy installation and allowing the use of industry-standard couplers to match any end-user’s requirements. Made from high-density polyethylene, the Standard Dimension Ratio (SDR) 11-rated inner chambers provide ample protection for all cables and are ideally sized for the installation of standard all-dielectric fiber cables up to 144-count. The robust design of ConQuest® Detectable SubDucts permits the use of standard fiber-optic cables construction rather than micro cables.

Furthermore, the design can be supplied with an optional integrated 18-gauge copper clad steel tone wire, allowing for the easy locating of all-dielectric fiber-optic cables. The outer jacket can be easily removed providing access to the inner ducts, allowing for easy installation and bending in confined areas such as underground pedestals. The conduit meets or exceeds the standards in ASTM D 3350-05 for Type III, Class PE 334480E (colors with UV stabilizer) or Class C (black), high-density polyethylene.

CommScope and ConQuest are registered trademarks of CommScope, Inc.

About CommScope

CommScope® (www.commscope.com) has played a role in virtually all the world’s best communication networks. We create the infrastructure that connects people and technologies through every evolution. Our portfolio of end-to-end solutions includes everything our customers need to build high-performing wired and wireless networks. As much as technology changes, our goal remains the same: to help our customers create, innovate, design, and build faster and better. We’ll never stop connecting and evolving networks for the business of life at home, at work, and on the go.

This press release includes forward-looking statements that are based on information currently available to management, management’s beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.

Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=6663612&lang=ja

News Media Contact:
Joseph P. Depa III, CommScope
+1 828-431-9803 or publicrelations@commscope.com
or
Lender Contact:
Phil Armstrong, CommScope
+1 828-323-4848