What_is_QAM_ImageThis blog post is part of a series called “CommScope Definitions,” in which we will explain common terms in communications network infrastructure.

QAM (quadrature amplitude modulation) is pronounced as a one-syllable word that rhymes with Guam. QAM has to do with the way that digital information is transmitted between two points.  Fundamentally, QAM enables an analog signal to efficiently transmit digital information. It also provides the means by which an operator transmits more bits in the same time period, which effectively increases the bandwidth.

QAM is a modulation scheme that transmits data by changing the amplitude, or power level, of two signals: first in-phase with the incoming data and the second 90 degrees out of phase. QAM relates to the number of bits of information encoded in each time period. For example, eight bits defines the number of combinations that are possible for those two signals (in phase and 90 degrees out of phase). If there are 256 combinations possible for those eight bits, then it is referred to as 256 QAM. Using a single time period to convey 10 bits would be 1024 QAM. 

In the cable television industry, QAM systems are used by multi-system operators (MSO) and other network operators to deliver video, voice and data services. QAM systems are the mechanisms that format services in hubs and headends, which are facilities where signals are processed and distributed over a cable system and to be delivered to subscribers’ homes where set top boxes, cable modems, and embedded multimedia terminal adapters (eMTA) convert the QAM signals back into useful voice, data and video.

Network operators are experiencing an ever increasing need for more QAM channels driven by the explosive demand by consumers for high-speed data, high-definition television, video-on-demand, network personal video recording, Internet Protocol cable television and digital phone service. From an overall cost perspective, QAMs matter to MSOs. They currently represent a significant portion of the capital spent for deploying digital video services. In the past, each individual service, such as high-speed Internet, broadcast cable television, and video-on-demand, had its own QAM modulator in a low density edge QAM. RF splitter/combiners were used to multiplex together the complete service line up. That led to racks and racks of QAM modulators and complex combining networks.

Wideband edge QAM devices have appeared to simplify the QAM modulator profusion. The QAM modulators evolved from managing individual services to managing multiple services and also from working with small groups of QAM carriers to supporting the entire 50 MHz–1 GHz spectrum on each port. A wideband edge QAM device is a dense, scalable solution that is vital to supporting additional advanced and next-generation services over HFC (hybrid fiber coaxial) networks. It enables cable operators and MSOs to integrate new service offerings seamlessly to support their business initiatives.

The current generation of wideband edge QAM modulators has incredible density—up to 2,560 QAM channels per chassis – and can manage all of the MSO-offered digital services across the entire downstream spectrum from each individual RF port.

Deploying a wideband edge QAM brings change and value to network operators. The evolution moves operators to a software-controlled platform from which to seamlessly add or reconfigure services, and it does that while reducing both their capital and operational expenditures. That combination is both exciting and rare.

Key Takeaway: QAM (quadrature amplitude modulation) is a modulation scheme used by network operators when transmitting data. QAM relates to a way of changing the amplitude, or power level, of two signals. QAM enables an analog signal to efficiently transmit digital information and increases the useable bandwidth.

Relevant Pages

About the Author

Shane Eleniak

Shane Eleniak is the Vice President of Advanced Broadband Solutions. With more than 20 years of experience in the telecommunications industry, Mr. Eleniak is responsible for leading CommScope’s Product Management and Engineering Development of Optical and Converged Access Solutions for the MSO Marketplace. Prior to joining CommScope, Shane was EVP of Marketing and Business Development for Alloptic where he guided product, sales and corporate strategy to deliver the industry’s first RFoG and DPoE solutions. While at Alloptic, Shane delivered solutions to over 50 MSO customers worldwide. Prior to Alloptic, Mr. Eleniak was Senior Vice President of Business Development for Corente, a privately held security and application management company, where he guided both product and corporate strategy. Mr. Eleniak was previously Vice President of Marketing and Sales for Corrigent Systems, the leader in packetized metro optical transport. He was responsible for creating Corrigent's marketing vision, developing their industry leading product strategy, managing worldwide customer and channel relationships and growing the company from conception to over $100M in revenue. Shane has previously held several key management positions in marketing, strategy, business development and engineering at such industry leaders as Centerpoint Broadband Technologies and Newbridge Networks/Alcatel-Canada. Mr. Eleniak holds a B.Sc. in Electrical Engineering (with distinction) from the University of Alberta

See all posts by this author

Add Your Comment

Please submit your comment using the form below

 
(required)  
 

Powered By OneLink