オーロラネットワークス( ANS)とRUCKUS®ネットワークスがVistance Networksに
すべての製品とコンテンツについては、新しいサイトをご覧ください。
オーロラネットワークス( ANS)とRUCKUS®ネットワークスがVistance Networksに
すべての製品とコンテンツについては、新しいサイトをご覧ください。
Wavelength Division Multiplexing (WDM) is a technique used in fiber optic communication that allows multiple data signals to be transmitted simultaneously over a single optical fiber. Each signal is assigned a unique wavelength of light, enabling independent data streams to coexist without interference. This method increases the capacity of fiber infrastructure without requiring additional fiber strands.
Multiple signals on a single fiber: WDM allows different data streams to travel simultaneously over one optical fiber by assigning each stream a unique wavelength, significantly increasing fiber capacity without laying new cables.
Two main types—CWDM and DWDM: Coarse WDM (CWDM) uses fewer, widely spaced wavelengths for cost-effective, short-distance applications, while Dense WDM (DWDM) supports many closely spaced wavelengths for long-distance, high-capacity networks.
Enhances Passive Optical Networks (PONs): WDM enables technologies like GPON, XGS-PON, and NG-PON2 to coexist on the same fiber infrastructure, allowing service providers to expand or upgrade networks without service disruption.
Passive components for signal management: WDM systems use optical multiplexers and demultiplexers to combine and separate wavelengths. These components are passive, aligning well with the energy-efficient nature of PONs.
Supports network evolution and service diversity: WDM enables more efficient fiber use, supports higher data rates, and allows multiple services to run over a single network—ideal for future-proofing broadband infrastructure.
There are two primary forms of WDM: Coarse Wavelength Division Multiplexing (CWDM) and Dense Wavelength Division Multiplexing (DWDM). CWDM uses fewer channels with wider spacing between wavelengths, making it suitable for shorter distances and cost-sensitive applications. DWDM supports a higher number of closely spaced wavelengths, making it ideal for long-distance and high-capacity networks.
In Passive Optical Networks, WDM is used to expand bandwidth and support multiple services over the same fiber. Different wavelengths can be assigned to different services or technologies, allowing systems like GPON, XGS-PON, and NG-PON2 to operate on the same infrastructure. This approach enables service providers to upgrade or expand networks without disrupting existing services.
WDM systems rely on optical filters to combine and separate wavelengths. A multiplexer (mux) at the transmitting end combines multiple wavelength channels onto a single fiber. At the receiving end, a demultiplexer (demux) separates the wavelengths, so each signal can be processed individually. These components are passive and do not require electrical power, which aligns with the architecture of PONs.
Using WDM in PONs allows for more efficient use of fiber, supports higher data rates, and enables the delivery of multiple services over a single network. It also provides a path for network evolution, allowing new technologies to be introduced alongside existing ones. This flexibility is especially valuable in areas where deploying new fiber is difficult or expensive.