Dual Band Antennas Go Full Circle

In this blog, CommScope's Donald Gardner explains how dual band antennas have come "full circle" using E-band frequencies to maximize capacity, coupled with microwave frequencies such as 23GHz to maximize availability for critical traffic.

There is an apocryphal story dating back to the early days of the telephone that claimed such newfangled technology would never take off. Why? Because there simply weren’t enough servants to pick up and answer the novel devices. A century later most of us now have our own personal ’servants‘ in the form of digital assistants.

I was clearing my desk recently and came across some old Andrew catalogues dating back to the 1980s and 1990s. These catalogues were like bibles to some and resided on almost every telecom engineer’s desk. The focus then was trunk radio solutions; microwave systems operating between 2 and 11GHz which relayed voice traffic across continents using large antennas between 8 and 15 feet in diameter. Mobile phones were the domain of a sharply dressed few.

CLICK TO TWEET: CommScope’s Donald Gardner explains how dual band antennas are a modern take on an old idea.

Thumbing through the catalogues, I came across some early dual band antennas and it struck me that certain industry challenges haven’t really changed all that much over the years. Dual band antennas were used to either free up space on towers or enable more capacity to be deployed without incurring the additional tower loads associated with installing another antenna.

Roll forward 30 years and long-haul trunk networks have largely been replaced with fiber while mobile communications and data access are now ubiquitous. Tower loading is still a major issue, as the demand for data requires the deployment of cellular antennas covering an ever-increasing number of bands. This, together with the associated filters and tower mounted amplifiers, along with microwave antennas to backhaul the traffic, stretches tower capacity to the limit.

The backhaul capacity is equally stretched – sites which could historically be connected with a single microwave channel now need two or more (and it is still often not enough). This has driven the industry to higher frequencies at 70 GHz and higher, where wider channels and dual polarized configurations allow capacity of up to 20Gb/s. There are trade-offs, as these E-band frequencies struggle with availability in poor weather conditions, thereby limiting the useable length of links.

This takes me full circle, back to the idea of dual band antennas from my old catalogues – only this time using E-band frequencies to maximize capacity (most of the time), coupled with microwave frequencies such as 23GHz to maximize availability for critical traffic. Check out the dual band antennas from CommScope – a modern take on an old idea.